Adding custom components
You can add a custom component in two ways: duplicating an existing component, or creating a new component.
To add a custom component by duplicating an existing component in the Graphics Editor:
- In the Power Operation folder, open the Graphics Editor.
- On the Graphics Editor screen, in the Components pane, find a standard component that is the same type as the custom component you want to create:
- ATS
- Breaker
- Meter
- Motor
- Source
- Switch
- Transformer
- Right-click the component, select Duplicate, and enter a unique name for the new custom component.
- Open the My Components category, right-click on the new custom component, and then select Edit.
- In the Objects pane, open the Group element and delete any figures (Line, Ellipse, etc.) that you do not want in the custom component. To maintain the existing advanced one-line animations, keep the Script and all Binds.
NOTE: You must keep the following:
- Rectangle Background
- Conditions
- The component ID prefix for the type you selected (Example: Breaker.MyCustomBreaker)
- All existing custom properties - Add or modify figures and connector points for the custom component.
A new instance of the Graphics Editor opens with the new custom component selected.